This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HB08-Q1: Query on Tj sense accuracy

Part Number: TPS1HB08-Q1

Tool/software:

Query is for the PN TPS1HB08AQPWPRQ1:

I understand from the datasheet pg no 27, current proportional to Tj is calculated using below formula,

In the Tj sense characteristics below (datasheet pg no: 7), we can see that there is min and max value and the tolerance is not constant across temperature range. May I know which parameter in the above formula affects this?

Can we get a way to find the tolerance for temperatures intermediate between two temperatures (eg: 25C & 85C)?

Thanks,

Sri Viswa