This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM83102: Application where Vout is same-as or close-to Vin

Part Number: TPSM83102


Tool/software:

Can the TPSM83102/103 act as a zero drop-out dc/dc regulator? In particular if Vin=3.3V and Vout=3.3V does the TPSM83102/103 achieve stable operation? Is type of application supported?

Also, what is the register default for Vout? Can I get device pre-programmed to have a particular default Vout value?

Thank you,

-Mark

  • Hi Mark,

    Our engineer is currently out of office, please expect a reply by next week Tuesday. Thank you for your patience.

    Best regards

    Yezi

  • Hi  Mark,

    Sorry for late reply bacause we are on Chinese public holiday from 1th OCT to 7th OCT.

    Yes, a zero drop-out application is absolutly ok for a buck-boost converter,  such as TPSM83102/3.

    Default Vout for both device is 3.3V, difference between TPSM83102 and TPSM83103 is the internal EN bit, 83102 is default disabled while 83103 is enabled.

    Then, you can configure the target vout you want before device start switching by TPSM83102.

    Regards

    Tao