Tool/software:
Hi,
I would like to understand the power rating required on below resistors. Please confirm if my understanding is correct.

1. Resistor for PG pin: Per datasheet, IPG is 100nA. Hence Power that the PU resistor need to withstand should be more than 100nA*100nA*100K=1nW
Hence in reality 0402 which can support 63mW is sufficient for Pull up.
2. Resistor for FB pin: Per datasheet, IFB is 70nA. Hence Power that the PU resistor need to withstand should be more than 70nA*70nA*680K=3.332nW
Hence in reality 0402 which can support 63mW is sufficient for Pull up.
3. Resistor for EN pin: Per datasheet, IEN(LKG) is 100nA. Hence similar to PG pin, PU 0-ohm Jumper which can withstand more than 100nA is sufficient.
Thanks