This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76202-Q1: Use as 2A overcurrent protecion and switching inductive loads

Part Number: LM76202-Q1

Tool/software:

Hi,

my customer is looking for a switchable output with 2A/24V which is short-circuit proof since it is an end-customer interface. In a previous project, they used the LM76202-Q1 ideal diode for overcurrent protection without reverse polarity protection.

Is it possible to operate the LM76202-Q1 device as a 2A overcurrent protection and switch on/off inductive load like fans via SHDN?

Best regards