Tool/software:
Hello,
I'm working on flyback converter design using the LM5156, and I am running into some issues. The design is a second side regulated isolated flyback designed to output 12V from a typical input of 24V. However, it is instead a sawtooth wave with a DC offset around 12V with a 3.5V amplitude. According to my output capacitor calculation, it should be 100mV. I therefore concluded it had something to do with the loop compensation circuit, but changing values here had no effect either. In fact, it only made it worse. Any suggestions on how to debug this problem?