This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
SM72442 has a circuit in its demo board (SM3320) where there is a boost startup circuit for when battery voltage > panel voltage.
SM72445 on the other hand, does not have such circuit in its datasheet or its application note. Given the info in table 2 of SM72445 datasheet where there is discussion on starting boost ratio of 1:1 or 1:1.2, do we still need the boost startup circuit if SM72445 used?
Other question is, what are the min and max duty cycles possible with this chip?
Hello Alinaghi,
As far as I can see, your expectation seems to be correct, but I am not 100% sure. Do you have some SM72445 which you could use on the SM3320 for checking it out?
For the other question: As this is not given in the datasheet, I cannot answer this question at the moment. I will try to find some information on it, but it might be difficult to get it. A test on the SM3320 might be the fastest way to get a typical value.
Best regards,
Brigitte
I ordered some SM72445 and put them on SM3320. The startup behavior was the same, and converter needed a boost kick signal, otherwise boost operation would not start.
Thanks for the suggestion on the second question. Will try some experiments to find out min and max duty cycle.
Hello Alinaghi,
Thank you very much for the feedback on the startup.
When checking some measurements on the SM3320 board, I have seen on-times of the low-side switch in the range of 400ns. I do not know if this is the minimum on-time, but possibly this is a starting point for you.
Best regards,
Brigitte