Tool/software:
Hi Ti,
Does the OTG function of the BQ25611D-EVM only support OTG when it is in high mode, or can it support both OTG and USB charging simultaneously?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Ti,
Does the OTG function of the BQ25611D-EVM only support OTG when it is in high mode, or can it support both OTG and USB charging simultaneously?
Hello,
The converter runs in buck mode from the input to the battery or boost/OTG mode from the battery to the input. It does not transfer energy simultaneously in both directions.
Regards,
Mike Emanuel