Other Parts Discussed in Thread: ALLIGATOR
Tool/software:
Dear Support,
I'm having difficulties in using the EVM for TPS48111Q1. I'm trying to drive loads at 24V, in the following conditions:
- No load using precharge path: output works correctly
- 100 ohm load using precharge path, with 100ohm connected after precharge completes: output works correctly
- 100 ohm load using precharge path, with 100ohm connected at startup: precharge works up until a level, as expected, then turning on the load triggers current fault (I guess too much current is still drawn into the load capacitors)
- 1 ohm load using precharge path, with 1 ohm load connected after precharge completes: turning on the load triggers current fault
The board is configured as follows:
- 50A current protection (no changes if current protection is completely disabled, so i guess ISCP triggers protection)
- tested also without input capacitor C16 (in order to read the real current input from the power supply), no current spike detected coming from power supply
I can't understand why the board can't drive the 24A to the load without triggering protection. No current spikes are present on both inputs and outputs.
Here the example with 1 ohm load connected after precharge has been completed (condition 4):
Yellow: Vin
Red: Vout
Blue: Iin
Green: Iout
Thank you,
Kind Regards