Other Parts Discussed in Thread: BQ78350
Tool/software:
Dear TI Team,
I am wondering if setting EDV_CMP to 1 takes into account self-discharge and electrical load settings to adjust the State of Charge.
Specifically, if a pack is going be sitting idle for some time, I would expect the voltage to decrease due to self discharge from the cells and the BMS electronics.
Will the state of charge adjust (decrease) accordingly to account for this? For example, if a pack is at 50V and 90%, and self discharges to 48V, will the fuel gauge still read 90% or will is decrease accordingly?
I also see there is a Self Discharge Rate parameter. Is this used to account for loads that aren't going to be seen by the sense resistor? Mainly, the load of the BMS electronics on the cells?
Thanks,
Kevin K