Other Parts Discussed in Thread: LM25149-Q1
Tool/software:
Hello TI
I am currently working with a team that is trying to design a power distribution board for a mars type rover, we are planning on using a 48V battery as our main power source and were looking into Buck converters to step down the voltage for our smaller electronic components. At the moment we are thinking that we will need about 7 or 8 of these to step down to the voltages of 24V with current draw of 2A, 15V with current draw of 10A, 12V with current draw 3A, 9V with a current draw of 3A, 5V with a current draw of 3.5A and another 5V with a current draw of 500mA and 3.3V with a current draw of 500mA. Also I saw that in the data sheet that this converter controller could be controlled with external circuitry are there any additional examples of circuitry that could fit our step down voltages? Also would you say that this controller would be good for our application or would you recommend we go with a different converter, if so which one?