This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: Battery not charging, MPPT disabled

Part Number: BQ25504


Tool/software:

Hi - my battery isn't charging from the solar panel (SOLAR CELL 87.6MW 3.4V).

I've tried it with a 150mAh (starting at 3.507V) and a 500mAh LiPo battery (starting at 3.859V).

Each time the battery voltage seems to rise about 10mA but no further.


I measure 3.2V at VIN_DC.
MPPT is disabled.

I appreciate any ideas!