Tool/software:
Hi,
I had a quick question regarding the TPS6508640RSK. When looking at the datasheet, the example shows the DRV5V rails as connected to LDO5, however we do say it can be powered externally. In the case I power it externally, am I allowed to power it up to 5V before VSYS is powered up to 15V? From my interpretation of the datasheet/device block diagram, this seems like it would be ok, but the device still wouldn’t output until VSYS is powered up. Is there anything else I would need to keep in mind when powering the DRV5V rail externally?
Thank you,
Matthew Bavier