This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
In table 5-1 Pin Functions it says that for PIN 5 DRTN, "Do not connect to PGND or AGND".
In Figure 8-18 PCB Layout Recommendation it says on the thermal pad "Connect DRTN to Thermal Pad". It also says to "Connect AGND to Thermal Pad".
Therefore DRTN would be connect to AGND.
Which is correct? The Pin Function table or the Layout Recommendations.
My apologies for the confusion, the comment in Figure 8-18 was suppose to be removed. Note: There is no connection from DRTN to EP (which is PGND) in the graphic.
The Bulleted List of the Layout Guidelines and the Pin Functional table are correct. The graphic note is an error.
Pin 5 - DRTN is the digital bypass return. It should not be connected to any net except the negative terminal of the BP1V5 bypass capacitor.
Do not connect it to AGND
Do not connect it to PGND
Do not connect it to GND
DRTN is internally connected to AGND, but must not be externally connected to another ground.