Tool/software:
Hi TI team,
We have custom requirement where we want to disable and enable short circuit protection during runtime.
By default our settings are enabled as follows:
(Shunt res- 0.1mohm
SCD threshold- 200 A)
We want to disable short circuit after first short circuit is encountered.
and there we are keeping following settings:
These settings are successfully disabling the protection without entering CONFIG_UPDATE mode.
There we observed the settings are not reverted back.
We also tried to reenable the setting by entering and exiting into CONFIG_UPDATE mode. But in this case, DDSG pin is going low which is disabling my DFET.
Now our requirement is to not to turn OFF DFET/DDSG pin and enable the settings again, which we are unable to handle. Can you help us out with that