This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62150A: SW pin absolute maximum ratings

Part Number: TPS62150A


Tool/software:

The SW pin MAX in TPS62150A datasheet 7.1 Absolute Maximum Ratings states "VIN + 0.3V", but this may be exceeded due to the voltage charged in the external capacitor, such as when the power is turned from ON to OFF. Is it correct to assume that this regulation applies only when the VIN voltage is normal (VIN=3 to 17V)?