Tool/software:
The TPS7A3001-EP data sheet indicates the reference voltage is Minimum -1.22V, Nominal -1.184V and maximum -1.142V. The graph in figure 2. shows VFB being near -1.175V at 25C. There appears to be an offset between the Vref and VFB. Can you clarify?
Does overall accuracy include the variation in Vref? The reference appears to have a variation of 3%, but overall accuracy, with load regulation effects is +/- 2.85%
Thanks