Tool/software:
My board is working in 4-20mA current loop. So the board should turn on at 3.6mA(10V). But while connecting this part the input voltage at 3.6mA reduced to 4.4V.
I had several debugging processes still it shows the same. Initially by increasing the input capacitance by 47uF and it started working. But after several days all the boards were stopped working.
So today I did one more test disabling the regulator (Pull down the Enable pin) that time the voltage is fine at 3.6mA shown 10V.
So I tried enabling the IC by keeping it off during the powerup that time its worked but after some time the output voltage reduced to 0.5V from 3.3V, the input voltage also reduced from 10V to 4.4V.
So please help me to resolve the issue as soon as possible