This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335A: 22V to 20V 3A

Part Number: TPS54335A
Other Parts Discussed in Thread: TPS563300

Tool/software:

I wanted to test my design using the WEBENCH website. However, the only voltage that the buck can be designed to outputs is 5V. I assume based on the data sheet and forum threads that it can be designed to output up to 30V at 3A? If it can, can WEBENCH be updated to reflect this change? Assuming the buck can output more then 5 volts can it convert 22 VDC to 20 VDC 3A?