Tool/software:
Hi,
I would like to connect two/three Battery Packs with high side 100V N-FET configuration bq76952 BMS for each. I have following questions
1. Is it safe to do so?
2. In 3 Series configuration , if middle most Battery hits Under voltage condition, after turning on charger for entire Pack will load detection work?
Thanks & regards
Mounish