This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62065: TLV62065

Part Number: TLV62065

Tool/software:

I have choosed this module , but there is no calculation for output current. This module can provide upto 2A current but my other modules are operate in different current. How TLV62065 give output current for different output current rating. i have 5 IC with different Current rating how to calculate correct current for Iout 

  • Hello Abdul,

    thanks for reaching out in E2E.

    Do you mean the 5 ICs are powered in parallel from the output of the TLV62065? In this case the load current of the TLV62065 is the sum of all attached ICs input currents.

    If the 5 ICs are in a different constellation then please provide more details.

    If this is a new design then I would suggest to consider one of our newer devices, such as TPS62825. Or do you have a special reason for choosing TLV62065?

    Best regards,

    Andreas.