Tool/software:
Hello team,
Customers want to select a variant for Output current=12A, Start-up voltage=0.800V, is TPS62872Y1QWRXSRQ1 which marked as yellow a right choice?
Thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello team,
Customers want to select a variant for Output current=12A, Start-up voltage=0.800V, is TPS62872Y1QWRXSRQ1 which marked as yellow a right choice?
Thanks!

Hi Daniel,
Yes, TPS62872Y1QWRXSRQ1 is the appropriate device to support the customer application. Actually, there are two options for this part to achieve a 0.8V output. Either connect a VSEL pin with 6.2kohm to GND or 4.7kohm to VIN.
What is the end of equipment and the system load? Is it to power an SoC?

Best regards,
Excel
Hello Daniel,
Do you have further queries? If not, can you kindly close the thread now?
Thank you.
Best regards,
Excel