This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23881B: Which values of R_AUTO have to be used (if using without MCU).

Part Number: TPS23881B

Tool/software:

My issue deals with input: AUTO (Pin#52). I will use this device without MCU.
Datasheet mentions: "R_AUTO enables autonomous operation at selectable port power allocation levels."
There is no description of these resistor values (selectable port power allocation levels) in the datasheet.
Question: Which values of R_AUTO have to be used?