This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS630702EVM: 5Vout efficiency curve not matching datasheet spec

Part Number: TPS630702EVM

Tool/software:

Hi, 

I am evaluating TPS630702 for my design. However, I am not able to get same efficiency as shown in datasheet. 

I am supplying 5.2V at input and have adjusted the output to 5V.

Please find following datapoints for your reference.

Vin  Iin (ma) Vout  Iout (ma) Efficiency Power D (mW)
5.2 10.22 5 10 94% 3.14
5.2 15.48 5 15 93% 5.50
5.2 20.78 5 20 93% 8.06
5.2 26.10 5 25 92% 10.72
5.2 31.47 5 30 92% 13.64
5.2 36.90 5 35 91% 16.88
5.2 42.21 5 40 91% 19.49
5.2 47.70 5 45 91% 23.04
5.2 53.14 5 50 90% 26.33
5.2 58.58 5 55 90% 29.62
5.2 63.85 5 60 90% 32.02
5.2 69.40 5 65 90% 35.88
5.2 75.00 5 70 90% 40.00
5.2 80.70 5 75 89% 44.64
5.2 86.40 5 80 89% 49.28
5.2 92.50 5 85 88% 56.00
5.2 98.00 5 90 88% 59.60
5.2 103.50 5 95 88% 63.20
5.2 109.20 5 100 88% 67.84
5.2 120.60 5 110 88% 77.12
5.2 132.40 5 120 87% 88.48
5.2 143.00 5 130 87% 93.60
5.2 153.70 5 140 88% 99.24
5.2 165.40 5 150 87% 110.08
5.2 177.10 5 160 87% 120.92
5.2 193.60 5 170 84% 156.72
5.2 204.00 5 180 85% 160.80
5.2 215.20 5 190 85% 169.04
5.2 227.60 4.99 200 84% 185.52
5.2 243.80 4.99 210 83% 219.86
5.2 255.00 4.99 220 83% 228.20
5.2 266.80 4.99 230 83% 239.66
5.2 278.60 4.99 240 83% 251.12
5.2 291.50 4.99 250 82% 268.30

Please let me know what changes needs to make on eval board for improving the output voltage efficiency.

Regards,

Anurag