This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23525: +48v source select

Part Number: TPS23525
Other Parts Discussed in Thread: TPS2411, LM74800-Q1

Tool/software:

Hello, I am looking for a power path selector similar to the TPS23525 but I need it to work for +48v instead.

We will have two +48V inputs that need to supply up to about 30A. We would like one input to be prioritized if possible and the other would only switch in if the first is OV/UV/etc.

Do you have a part that can handle this?