Other Parts Discussed in Thread: BQ40Z50, BQ34Z100
Tool/software:
Hi
I am currently considering a battery circuit using the URB12200 Battery pack (12.8V 20Ah LiFePO4 Li-ion), and customer support recommended the BQ40Z50-R2.
Is this IC capable of cell balancing when connecting two batteries in parallel?
The datasheet states that the maximum VC1 rating is 8.5V or VSS+30V, so I feel it would be difficult to use a 12V battery.
Please let me know the best IC, including this one.
Best regards