Tool/software:
Hello, I have voltage Uin=42V and Uout=24V. The connection is Rfbt=100k, Rfbb=4.3k, L=47uH, Cout= 4*22uF. When the output is loaded from 250mA to 2A, I have a ripple up to Uout=50mV. If I do not have a loaded output, then I have a ripple of Uout=130mV. Where can the problem be?