Tool/software:
Hi there
VatChgTerm is set incorrectly in our app(Should be 4400mV, but incorrectly set to 4252mV), causing the FCC to drop on first charge. We measured it and the FCC dropped, but the RM did not.
May I ask if there are any other parameters other than VatChgTerm parameter setting error that can cause similar phenomenon when FCC changes but RM doesn't? If so, please help to list them.
我们应用程序中的 VatChgTerm 设置不正确(应该是4400mV,错误的设置为了4252mV),导致首次充电时 FCC 下降。我们进行了测量,FCC 下降了,但 RM 没有下降。
请问,除了 VatChgTerm 参数设置错误外,是否还有其他参数会导致 FCC 变化而 RM 不变的类似现象?如果有,请帮忙列出。