This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC24624: Transformer Design

Part Number: UCC24624


Tool/software:

Hi TI members,

I need to design a Center-tapped Transformer similar to the one in the document: "UCC24624 Dual-Channel Synchronous Rectifier Controller for LLC Resonant Converters"  from TI. Please advise how I can design this transformer according to my specifications.

The spec values are:

Input Voltage: 60V

Output Voltage: 30V

Turns ratio = 2 : 1

Switching Freq range: 0-160Khz

Resonant Frequency: 55 / 60Khz LLC Converter

Output Power:  150Watt (30V output x Max Cuurent 5A).

Is there any online tool or simulator through which i can put those above values and then get the result like transformer core size, wire gauge of the windings, core and wire cross-section area and other parameters for designing the Center tapped transformer?

Please Suggest accordingly

Kind Regards

Arsalan