Part Number: TPS61094
Other Parts Discussed in Thread: LM66100
Tool/software:
Hi TI Team,
we are already using the TPS61094 in an application.
Now, we have the requirement, to generate a higher power output in backup mode (boost operation).
Requirements for Backup Mode:
Output voltage: 4.5V
Output current: 500 mA
We want to use only one SuperCap, due to size limitations and costs.
I'm curious to know, if it is possible to connect directly two or even three TPS61094 in parallel on the VOUT?
Due to slightly differnces in the VOUT voltage, is there a reverse current to expect?
Should both TPS61094 be decoupled with an ORing (ideal diode e.g. LM66100)?
Since the TPS61094 doesn't have a FB input, that can be shared, only OSEL could be set equal.
Should OSEL be connected to the same resistor, if running in parallel? I don't think so...
Thanks for your answer in advance,
Christian