Tool/software:
Hey Multiphase Buck Team,
I have a customer evaluating the TPS40090 for a new project and we were hoping you could help to provide feedback on the inquiry below!
It is our understanding that if the CS inputs go beyond 100mv then then there is a degradation in accuracy. Our interpretation of this is that if the CS signals go beyond 100mV then the there is non-linearity of the gain value. Can TI provide a curve that shows the “g” gain over the range of CS voltages from 0V to 200mV? If it turns out that it is not the current amplifier gain that causes the inaccuracies, then we would still like to understand the possible variance out to 200mV.
-Matt