Other Parts Discussed in Thread: CSD16340Q3, CSD17575Q3
Tool/software:
Hi support team,
I changed the EVM's peripheral constants and the operation check went well.
However, when I produced a prototype board, it didn't work properly.
The output voltage itself is the expected boosted voltage,
but the following is happening:
- The gate voltage of the H-Side FET is low. (The H-Side FET is not turned on.)
→ The bootstrap circuit is not functioning?
- The switching frequency is slow.
→ The resistance of the RT pin is correct (100kΩ).
- The L-Side FET is outputting H at an unexpected time.
Please let me know if you have any suggestions.
It is drawing a 6A load.
It is not in DCM at a light load.
It seems like the HDRV output is simply not being output,
but are there any conditions that would stop the HDRV output?
(If not, is it simply broken?)
Regards,
Dice-K