This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3435: Watch Dog IC Recommendation Inquiry

Part Number: TPS3435

Tool/software:

Hi, TI expert.

A customer has requested a Watch Dog IC recommendation.

1. Input voltage 5V
2. After booting, if there is no signal (GPIO HIGH or LOW) from the MCU for a certain period of time (approximately 0.1s to 10s), change DC-DC Enable to LOW and then change it back to HIGH (Power Reset)
3. Timer Variable Type

After checking the above, please recommend a suitable Watch Dog IC (Reset IC).

Please check. Thank you.