This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS389C03-Q1: Alternative for MAX20478BATBH/VY+

Part Number: TPS389C03-Q1

Tool/software:

Hi team, 

Would like to check with you if we have P2P alternative for MAX20478BATBH/VY+. If not, please also recommend our non-P2P alternative.

Thanks!

Ethan Wen

  • Hello Ethan, 

    I see the MAX20478 device is a ASIL D multichannel supervisor with watchdog. Currently we have TPS389C03-Q1 released which is a ASILD multichannel supervisor with Q&A watchdog. We are able accommodate multiple channel counts, though we are not directly pin to pin. If a window watchdog is required this will fall under our TPS388C0x-Q1 device, which is ASILB at a device level. 

    1. What is the desired ASIL rating?

    2. What application is this in? 

    Please feel free to email me directly if response contains sensitive information. 

    Regards, 

    Oscar Ambriz 

  • Hi Oscar, 

    Thanks for the feedbacks. 

    The desired ASIL rating is ASIL-B. The application is the cockpit, and use for monitoring MCU's safety related power rail(2 to 3 rails, 1.2V/1.8V/3.3V). 

    I don't find detailed information/schedule for TPS388C0x-Q1 information in ti.com. May you kindly provide that? 

    Ethan Wen

  • Hi Ethan, 

    Since Oscar is currently out of office, I will support you from now on. I will reach out to you via email to provide more information 

    Best, 

    Sila