Tool/software:
Hi,
I would like to know the values of input low current (IIL), input high current (IIH), output low current (IOL), and output high current (IOH) for TPS3852-Q1.
Thanks & regards
Priyanka S P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I would like to know the values of input low current (IIL), input high current (IIH), output low current (IOL), and output high current (IOH) for TPS3852-Q1.
Thanks & regards
Priyanka S P
Hi Priyanka,
We do not have values for the input low current (IIL) & input high current (IIH) as the inputs are voltage threshold level based.
The output low current and output high current are based on the pullup voltage and current as this is an open drain device. The device recommends keeping these values below 10mA.
Thanks,
Joshua