Tool/software:
Hi,
I'm working on an application similar to that described here:
I'm using a TPS25762 to build a "sourcing device". The CC1, CC2, Vbus pins on the USB-C port will be connected to the TPS25762, while DM and DP will be connected to a microcontroller (actually an external ULPI PHY) which will act as a USB2 device. It sounds like this will require the 762-Q1 to issue a Data Role Swap command after negotiation. Is it possible to set this up with the '762 GUI?