This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: I2C address shifter

Part Number: BQ76930

Tool/software:

Hello,

I would like to use more BQ76930 ICs on the same I2C bus. Since mentioned IC has fixed I2C address there is an I2C address shifter needed, like LTC4316. In a datasheet of LTC4316 is written that: 

----------------------

The LTC4316 is designed to support most I2C and SMBus message protocols. The only exceptions are protocols that use pre-assigned addresses on the slave side of the bus.

Unsupported I2C Protocols: 10-Bit Addressing, Device ID, Ultra Fast-Mode I2C Bus Protocol

-----------------------

Would BQ76930 work with LTC4316 or does it look incompatible?

Many thanks, Kind regards, Dejan.