Tool/software:
I have completed a couple of cycles but they always end with UpdateStauts as 0x0D. I do not expect UpdateStauts to be greater than 0x06 according to the TRM pg 151.
I do see the RDIS flag clearing after first discharge.
During Charging, the FC flag is set
During Discharging, the FD flag is set
I do see the VOK flag clearing during the rest after Charging and Discharging.
A capacity is learned that is different than the nominal. I see the Qmax change from 1050mAh (nominal) to around 1030-1060mAh
CHEMID: 7539
The pack is a 2S1P
Cell is RouteJade SLPB593459HP1
Charge Parameters
8.4V, 525mA taper is 50mA
Discharging Parameters
5.4V 210mA or 150mA
I can provide logs.