Tool/software:
Hello,
I have designed a circuit using the BQ25792 IC to charge a lithium polymer battery and supply power to the system through the voltage output from the SYS pin. However, the battery is not charging, although the output voltage at the SYS pin is normal. Could you please review the circuit?
- No operation I2S.
- D + and D- pins not used.
- VBUS Input voltage are 15V
- SYS Pin output are 7.2V
- The PROG BAT , 2S and 1.5MHz (li-polymer battery , Nominal Voltage 3.7V)
- The circuit does not do any boost or buck.
Thank you.