This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS922055DRRREVM: Current Limiting Issue

Part Number: TPS922055DRRREVM


Tool/software:

  1. I am using the TPS922055DRRREVM eval board and I am unable to limit the current. I am using an off the shelf LED strip rated for 12V, 1A. My external power supply is set to output 18V and is capable of 1.5A. I have replaced the 50mΩ resistor (R1) with a 200mΩ to limit the current to 1 amp. ADIM/HD and PWM are both tied high using the provided jumpers. When I connect everything and power the board up, my current consumption shoots to 1.5A.

  2. I can’t seem to get the red fault LED to turn off and I have verified that I am not in violation of any criterion as shown in table 8-3 of the TPS92205x datasheet.