This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18531Q5A: Maximum Leakage Current

Part Number: CSD18531Q5A

Tool/software:

What is the maximum leakage current over temperature for CSD18531Q5A

  • Hello Christopher,

    Thanks for the inquiry. There are two leakage specs in the datasheet: IGSS < 100nA at VDS = 0V, VGS = 20V and T = 25°C & IDSS < 1μA at VDS = 48V, VGS = 0V and T = 25°C. Final test is done at 25°C and there is no elevated temperature testing. I pulled up the characterization data collected during product development -55°C, -25°C, 25°C, 75°C, 125°C and 150°C. Max IDSS ~38μA at 150°C and max IGSS ~ 40nA at 150°C. Please note, this is for design guidance only and TI only guarantees what is specified in the datasheet and tested in production. Please let me know if you have any questions.

    Best Regards,

    John Wallace

    TI FET Applications