Tool/software:
I want to use UCC24624EVM-015.The configuration of our system is half bridge.The current rating of our system's diode is more than 220A.Now we want to switch to synchronous rectification.Output voltage we are expecting is 48V.Load is 10.5KW.Frequency of our transformer is 30kHz+-12kHz.Can I use this for our system. If yes, then what are the changes that I have to do?