Tool/software:
Hello,
I am charging a battery using a charger current of 480mA (ISET). Based on the datasheet, the charger termination current should be 10% of this value (48mA) with an error of 10%. However, I am getting an error higher than this 10%. The IC is terminating the charging process around 70mA (this value is constant). Due to this error, the fuel gauge never reaches 100%.
I have another PCB with this charger IC working properly, stopping the charging process at around 45mA.
Is this error normal? What can I do to fix it?
Thank you.
Best regards,
João Rego