Tool/software:
Hi Sir,
I'm working on a battery-protected design using the BQ29733.
The goal is to prevent primary battery passivation, so we need to incorporate a parallel HLC (Hybrid Layer Capacitor).
In our scenario, the user can remove the battery, but the HLC remains embedded inside the DUT.
The reason for using the BQ29733 is to prevent the HLC from powering the system when the battery is removed.
I've attached the schematic, and I observed that the BATT+ voltage(primary battery) remains at the same level as the HLC(BATT-3.6V), keeping the system alive even after the battery is removed until the voltage drops to 2.8V.
Does this meet your expectations?