Tool/software:
Hi,
I am using the circuit diagram in the attachment. I aim for an input voltage range of 13-32V. The output voltage will be 5V. The current drawn is at 100mA.
I am currently experiencing a problem. When I apply 24V to the TPS5410 input and current of 60mA at 5V at its output, the TPS5410 heats up. The body temperature exceeds 40 degrees Celsius. The input current is approximately 30mA.
I also replaced the 30uH inductor in the circuit with a 100uH. But I could not reduce the heat.
What is the problem in this schematic and how can I solve it.
Best regards,
Osman

Note: # marked materials were not installed