This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC14240-Q1: boostrap

Part Number: UCC14240-Q1

Tool/software:

Team,

is one UCC14240 able to offer 3 bias powers with boostrap circuitry to drive upper IGBTs? If so, could you offer ref. design! Very thanks. 

application: AC inverter

Regards

Brian

  • When considering power level, regulation accuracy, inrush current and HV safety isolation, the proposed configuration is not recommended with UCC14240. Depending on required power level and max ambient temperature, it may be ok to use a single UCC1420 for biasing three low-side referenced gate drivers (GD2, GD4, GD6).

    Steve