This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55383: Maximum current in operation mode

Part Number: TPS55383


Tool/software:

Hi,

I use TPS55383PWPR for buck converter from single input of 24V to two outputs 5v & 5.5v.

In the datasheet I'm don't understand what is the maximum current of the two outputs.

In the obsolete values table write 7A, and in the operational table write 4.5A of output1 and if i use BP in output2 is also 4.5A.

I would like to your help.

Best Regards,

Dror