Other Parts Discussed in Thread: TPS22929D
Tool/software:
Hi Team,
May I have your help to provide pin-to-pin suggestions for below competitor?
Thanks.
AP22913W6-7
AP2280-1WG-7
AP2280-2W
AP2281-1WG-7
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi peter,
Can you confirm if you want alternative in SOT packages or in other packages or both packages are fine as long as they are p2p. I see that all these AP devices come in different packages and the part number you have mentioned are SOT packages but still wanted to confirm once.
Best Regards,
Arush
Hi Team,
Sorry for confusing you..
Since there are 4 devices that I want to replace, I need p2p suggestions for each of them!
Please help.
Thanks.
Hi Peter,
AP22913W6-7
TPS22929D. This is the only device which I found to be having SOT package and is p2p with this device.
AP2280-1WG-7
No p2p SOT alternatives
AP2280-2W
This has same package as AP2280-1WG7 (they are same device with only rise time difference). No p2p.
AP2281-1WG-7
This one has common package with AP22913W6-7 so TPS22929D should also work here.
Best Regards,
Arush
These are all SOT package cross referencing. We have some options in WSON or DSBGA packages but I did not mention them here as the part numbers which you shared are all SOT (these devices so come in other package).
Best Regards,
Arush