Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hello,
I've attached the file I'm using to simulate as well as the google design sheet provided by TI.
A couple of specs:
Pout = 500W
Vout = 400VDC
Vin = 410VDC
I've used the excel sheet to get started and tried not to change a lot in the provided tina-ti simulation.
I've got no-load attached to the secondary. To make sure it regulates I've used a very slow controller that should easily regulate with no load, yet it doesn't.. Some insight into why I'm having difficulties would be great. I've used suggested values from the excel sheet and designed the converter for somewhere between Vout_max and Vout_min.
If you could look into the file and see why the converter is not regulating even with such a slow loop, that would be great.