This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H160-Q1: Drive multiple loads from 12V car battery

Part Number: TPS4H160-Q1
Other Parts Discussed in Thread: TPS4H000-Q1

Tool/software:

Can TPS4H160-Q1 be directly connected to car battery as Vin to drive loads? Will power surges cause issues? We plan to use following schematic between car battery and TPS4H160. The loads are mostly detection/trigger wires like ACC, REV, ILL for car head units which draws less than 200mA. Are there better IC more suitable for the application?