Other Parts Discussed in Thread: BQSTUDIO, BQ76942EVM, BQ34Z100EVM, GPCCHEM
Tool/software:
State of Charge is only accurate during the charge cycle. Remains at 100% when I discharge the battery.
1) I'm using 3 Lithium Polymer batteries from MOTOMA. (No Chem files available but 3.7V 3400mAh) They are connected as a Pac on a BQ76942EVM but I've bypassed all the FETS on that board to test the BQ34Z11xxEVM board. The Power supply is connected to BAT+ and PACK- and the electronic load is connected to BAT+ and BAT-. I've entered the FCC value of 12600mV, the number of cells (3) and set the VOLSEL bit. I've calibrated the Voltage and the Current and BqStudio accurately displays the voltage and the Average current during charging. Also, during charging the SOC is correct and the WAKE button illuminates the LEDs correctly. However, when I disconnect the charger and apply a load the Average Current goes to zero and the SOC remains at 100%. I've cycled this several times. I'm sure this is user errro but any insight would e appreciated.